- Home
- Company
- News
- Press Releases
- 2023-FX_3-A
Simplified welded steel fastening
Introducing the FX 3-A Cordless stud fusion system, helping revolutionize fastening on steel
OAKVILLE, ONTARIO (Aug. 1, 2023) – In the natural resources and shipbuilding industries, high-quality welding, bolting, and clamping can be considered an art. Additionally, skilled labor continues to be in high demand, affecting the overall cost and delivery of projects. Hilti North America, a global leader providing innovative tools, technology, software, and services to the commercial construction industry, recognized this as an opportunity for disruption—and developed the FX 3-A Cordless stud fusion system to help revolutionize fastening on steel.

The new FX 3-A Cordless stud fusion system cuts welding time significantly. Covering higher loads and thinner base materials than previous Hilti products, cordless stud fusion is up to 75% faster than traditional welding methods and is a fully mobile and autonomous system with no power cables needed.
This fastening method is also safer than traditional welding methods as it helps shield users from heat and gas. With virtually no sparks, splatters fumes and no angle grinder needed for the surface preparation, it offers more significant advantages from a health and safety perspective.
A wide range of end-user benefits
Compared to welding and other methods like bolting and clamping, cordless stud fusion allows more speed and flexibility in engineering, procurement, and construction.
Engineers know they will get more reliable loads–through repeatable and consistent fastenings–as well as more flexibility for design changes. When combined with modular systems like Hilti’s MT or Oglaend portfolios, this new fastening method enables greater use of supports. This is a result of the stronger connection to steel, which is often the weak point of supports with other methods like clamping.
Procurement can choose from a wide portfolio of studs with international approvals and corrosion resistance (up to C5 in highly corrosive environments). As a result, construction becomes not only faster than traditional methods, but it can also be done by almost anyone—with minimal training—helping to reduce the risk of installation error.
Collectively, the benefit of this system gives customers more flexibility and more capacity to finish the work earlier. It’s also a cleaner system with no welding slag, burn marks or ceramic ring waste. When using an optional sealing washer with S-BT-MR SN threaded stud, post-painting is not required. With the easier-to-follow H-code setting customers can expect higher-quality and more consistency, with repeatable fastenings. Additionally, the Active Fusion Indicator (AFI) gives the installer systematic real-time feedback to help improve the quality of fastening.
Norbert Tiringer
Hilti North America’s Director of Marketing for Energy & Industry

For additional information about cordless stud fusion, visit our Fastening to Steel editorial.
About Hilti North America
Hilti North America is a leading provider of higher quality, innovative and specialized tools, fastening systems and software-based solutions for the professional user. With more than 3,800 highly trained Hilti account managers, engineers, and Hilti employees throughout North America, Hilti’s expertise covers the areas of powder actuated fastening, drilling and demolition, diamond coring and cutting, measuring, firestopping, screw fastening, adhesive and mechanical anchoring, strut and hanger systems, solutions for tool crib productivity as well as worker health and safety.