SF BT 22‑A
Original operating instructions
Information about the documentation
About this documentation
- Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
- Observe the safety instructions and warnings in this documentation and on the product.
- Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
Explanation of symbols used
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the documentation
The following symbols are used in this document:![]() |
Read the operating instructions before use. |
![]() |
Instructions for use and other useful information |
![]() |
Dealing with recyclable materials |
![]() |
Do not dispose of electric equipment and batteries as household waste |
Symbols in the illustrations
The following symbols are used in illustrations:![]() |
These numbers refer to the corresponding illustrations found at the beginning of these operating instructions |
![]() |
The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text |
![]() |
Item reference numbers are used in the overview illustrations and refer to the numbers used in the product overview section |
![]() |
This symbol is intended to draw special attention to certain points when handling the product. |
Product-dependent symbols
Symbols on the product
The following symbols can be used on the product:![]() |
The power tool supports near-field communication (NFC) technology, which is compatible with iOS and Android platforms. |
![]() |
Hilti Li-ion battery type series used. Observe the information given in the section headed Intended use . |
![]() |
Li-ion battery |
![]() |
Never use the battery as a striking tool. |
![]() |
Do not drop the battery. Never use a battery that has suffered an impact or is damaged in any other way. |
Symbols
The following symbols are used:![]() |
Read the operating instructions before use. |
![]() |
Instructions for use and other useful information |
![]() |
Rated speed under no load |
![]() |
Revolutions per minute |
![]() |
Direct current (DC) |
![]() |
Diameter |
Illustrations
The illustrations in these operating instructions are intended to convey a basic understanding and may differ from the actual version of the product:![]() |
These numbers refer to the corresponding illustrations found at the beginning of these operating instructions. |
![]() |
The numbering in the illustrations reflects the order of the work steps in the illustration and may deviate from the numbering of work steps in the text. |
![]() |
Item reference numbers are used in the overview illustration. In the product overview section, the numbers shown in the legend relate to these item reference numbers. |
Product information
Hilti products are designed for professional use and may be operated, serviced and maintained only by trained, authorized personnel. This personnel must be informed of any particular hazards that may be encountered. The product and its ancillary equipment may present hazards when used incorrectly by untrained personnel or when used not as directed.- Make a note of the designation and serial number printed on the identification plate in the following table.
- Always quote this information when you contact a Hilti representative or Hilti Service regarding questions about the product:
Product information
Drill |
SF BT 22‑A |
Generation: |
01 |
Serial no.: |
Safety
General power tool safety warnings
![Image alternative](https://files-techDocs.hilti.com/2160456/H2_SYM-Hinweis_M_M_DEU_Gefahr.jpg)
Read all safety warnings and all instructions. Failure to follow the warnings and instructions may result in electric shock, fire and/or serious injury.
Save all warnings and instructions for future reference.
The term “power tool” in the warnings refers to your mains-operated (corded) power tool or battery-operated (cordless) power tool.
Work area safety
- Keep work area clean and well lit. Cluttered or dark areas invite accidents.
- Do not operate power tools in explosive atmospheres, such as in the presence of flammable liquids, gases or dust. Power tools create sparks which may ignite the dust or fumes.
- Keep children and bystanders away while operating a power tool. Distractions can cause you to lose control.
- Power tool plugs must match the outlet. Never modify the plug in any way. Do not use any adapter plugs with earthed (grounded) power tools. Unmodified plugs and matching outlets will reduce risk of electric shock.
- Avoid body contact with earthed or grounded surfaces, such as pipes, radiators, ranges and refrigerators. There is an increased risk of electric shock if your body is earthed or grounded.
- Do not expose power tools to rain or wet conditions. Water entering a power tool will increase the risk of electric shock.
- Do not abuse the cord. Never use the cord for carrying, pulling or unplugging the power tool. Keep cord away from heat, oil, sharp edges or moving parts. Damaged or entangled cords increase the risk of electric shock.
- When operating a power tool outdoors, use an extension cord suitable for outdoor use. Use of a cord suitable for outdoor use reduces the risk of electric shock.
- If operating a power tool in a damp location is unavoidable, use a residual current device (RCD) protected supply. Use of an RCD reduces the risk of electric shock.
- Stay alert, watch what you are doing and use common sense when operating a power tool. Do not use a power tool while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating power tools may result in serious personal injury.
- Use personal protective equipment. Always wear eye protection. Protective equipment such as dust mask, non-skid safety shoes, hard hat, or hearing protection used for appropriate conditions will reduce personal injuries.
- Prevent unintentional starting. Ensure the switch is in the off‐position before connecting to power source and/or battery pack, picking up or carrying the tool. Carrying power tools with your finger on the switch or energising power tools that have the switch on invites accidents.
- Remove any adjusting key or wrench before turning the power tool on. A wrench or a key left attached to a rotating part of the power tool may result in personal injury.
- Do not overreach. Keep proper footing and balance at all times. This enables better control of the power tool in unexpected situations.
- Dress properly. Do not wear loose clothing or jewellery. Keep your hair, clothing and gloves away from moving parts. Loose clothes, jewellery or long hair can be caught in moving parts.
- If devices are provided for the connection of dust extraction and collection facilities, ensure these are connected and properly used. Use of dust collection can reduce dust-related hazards.
- Do not force the power tool. Use the correct power tool for your application. The correct power tool will do the job better and safer at the rate for which it was designed.
- Do not use the power tool if the switch does not turn it on and off. Any power tool that cannot be controlled with the switch is dangerous and must be repaired.
- Disconnect the plug from the power source and/or the battery pack from the power tool before making any adjustments, changing accessories, or storing power tools. Such preventive safety measures reduce the risk of starting the power tool accidentally.
- Store idle power tools out of the reach of children and do not allow persons unfamiliar with the power tool or these instructions to operate the power tool. Power tools are dangerous in the hands of untrained users.
- Maintain power tools. Check for misalignment or binding of moving parts, breakage of parts and any other condition that may affect the power tool’s operation. If damaged, have the power tool repaired before use. Many accidents are caused by poorly maintained power tools.
- Keep cutting tools sharp and clean. Properly maintained cutting tools with sharp cutting edges are less likely to bind and are easier to control.
- Use the power tool, accessories and tool bits etc. in accordance with these instructions, taking into account the working conditions and the work to be performed. Use of the power tool for operations different from those intended could result in a hazardous situation.
- Recharge only with the charger specified by the manufacturer. A charger that is suitable for one type of battery pack may create a risk of fire when used with another battery pack.
- Use power tools only with specifically designated battery packs. Use of any other battery packs may create a risk of injury and fire.
- When battery pack is not in use, keep it away from other metal objects, like paper clips, coins, keys, nails, screws or other small metal objects, that can make a connection from one terminal to another. Shorting the battery terminals together may cause burns or a fire.
- Under abusive conditions, liquid may be ejected from the battery; avoid contact. If contact accidentally occurs, flush with water. If liquid contacts eyes, additionally seek medical help. Liquid ejected from the battery may cause irritation or burns.
- Have your power tool serviced by a qualified repair person using only identical replacement parts. This will ensure that the safety of the power tool is maintained.
Drill safety warnings
- Use auxiliary handle(s), if supplied with the tool. Loss of control can cause personal injury.
- Hold power tool by insulated gripping surfaces, when performing an operation where the cutting accessory may contact hidden wiring. Cutting accessory contacting a "live" wire may make exposed metal parts of the power tool "live" and could give the operator an electric shock.
Additional safety instructions
Personal safety- Use the tool only when it is in technically faultless condition.
- Never tamper with or modify the tool in any way.
- Always hold the tool with the hand on the grip provided. Keep the grip clean and dry.
- Avoid touching rotating parts – risk of injury!
- Wear suitable protective glasses, a hard hat, ear protection, protective gloves and light respiratory protection while using the power tool.
- Wear protective gloves also when changing the accessory tool. Touching the accessory tool presents a risk of injury (cuts or burns).
- Wear eye protection. Flying fragments present a risk of injury to the body and eyes.
- Take breaks between working and do physical exercises to improve the blood circulation in your fingers. Exposure to vibration during long periods of work can lead to disorders of the blood vessels and nervous system in the fingers, hands and wrists.
- Use a dust removal system and suitable vacuum cleaner whenever possible. Dust from materials, such as paint containing lead, some kinds of wood, concrete / masonry / stone containing silica, and minerals as well as metal, may be injurious to health.
- Keep the power tool out of reach of children. The power tool is not intended for use by inexperienced persons who have received no special training.
- Observe the national health and safety requirements.
- Do not use the battery as a power source for other unspecified appliances.
- Observe the special guidelines applicable to the transport, storage and use of lithium-ion batteries.
- Do not expose batteries to high temperatures, direct sunlight or fire.
- Do not disassemble, squash or incinerate batteries and do not subject them to temperatures over 80°C (176°F).
- Do not attempt to charge or continue to use damaged batteries.
- If the battery is too hot to touch it may be defective. In this case, place the power tool in a non-flammable location, well away from flammable materials, where it can be kept under observation and allowed to cool down. Contact Hilti Service after the battery has cooled down.
Description
Overview of the product
![Image alternative](https://files-techDocs.hilti.com/2160456/H2_BILD-Objekt_System_SF_BT_22-A-G1_DEU_SFBT22_Produktuebersicht_P3_00.jpg)
- Keyless chuck
- Motor cooling air intake
- Grip
- Switch safety lock
- Control switch (with electronic speed control)
- Belt hook
- Battery
- Air exit
- Battery release button
- Battery display
Intended use
The product described is a hand-held cordless drill designed for drilling blind holes in steel using Hilti TX‑BT… stepped drill bits which is a prerequisite for driving Hilti X‑BT threaded studs.
Use only Hilti lithium‑ion batteries of the B 22 series with this product.
Use only Hilti -approved battery chargers to charge these batteries. More information is available from your Hilti Store or from www.hilti.group
Switch-on interlock release button
![Image alternative](https://files-techDocs.hilti.com/2160456/H2_BILD-Objekt_System_SF_BT_22-A-G1_DEU_SFBT22_Einschaltsperre_00.jpg)
-
Switch positions
- If the switch safety lock is positioned longitudinally, i.e. in line with the working direction of the drill, the control switch is locked (the safety lock is active).
- If the switch safety lock is pointing to the left relative to the working direction of the drill, the control switch is free to operate (the safety lock is deactivated).
Overload and overheating protection
The power tool is equipped with an electronic system to protect against overloading and overheating. The power tool switches itself off automatically in the event of overloading or overheating. After releasing the control switch, the power tool may not restart immediately when the switch is pressed again (while the power tool is cooling down).Li‑ion battery display
The charge status of the Li-ion battery and malfunctions of the power tool are indicated by the display on the Li‑ion battery. The charge status of the Li‑ion battery is displayed after pressing one of the two battery release buttons.Status |
Meaning |
---|---|
4 LEDs light. |
Charge status: 75 % to 100 % |
3 LEDs light. |
Charge status: 50 % to 75 % |
2 LEDs light. |
Charge status: 25 % to 50 % |
1 LED lights. |
Charge status: 10 % to 25 % |
1 LED blinks, the power tool is ready for use. |
Charge status: < 10 % |
1 LED blinks, the power tool is not ready for use. |
The battery has overheated or is completely discharged. |
4 LEDs blink, the power tool is not ready for use. |
The power tool is overloaded or has overheated. |
Items supplied
Electric drill, operating instructions.Other system products approved for use with this product can be found at your local Hilti Store or at: www.hilti.group
Technical data
Rated voltage |
21.6 V |
Weight including battery B22⁄8.0 |
5.7 lb (2.6 kg) |
Torque |
≤ 7 ftlbf (≤ 9 Nm) |
Keyless chuck clamping range |
3/64 in … 25/64 in |
Operation
Inserting the battery
![Image alternative](https://files-techDocs.hilti.com/2160456/H2_BILD-Objekt_System_SF_BT_22-A-G1_DEU_SFBT22_AkkuEinsetzen_00.jpg)
- Push the battery into the drill from the rear until it is heard to engage with a click.
Removing the battery
![Image alternative](https://files-techDocs.hilti.com/2160456/H2_BILD-Objekt_System_SF_BT_22-A-G1_DEU_SFBT22_AkkuEntnehmen_00.jpg)
- Remove the battery.
Fitting the belt hook (optional)
![Image alternative](https://files-techDocs.hilti.com/2160456/H2_BILD-Objekt_System_SF_BT_22-A-G1_DEU_SFBT22_GuertelhakenMontieren_00.jpg)
- Fit the belt hook on the appropriate side of the drill.
Fitting or removing accessory tools
![Image alternative](https://files-techDocs.hilti.com/2160456/H2_BILD-Objekt_System_SF_BT_22-A-G1_DEU_SFBT22_Werkzeugwechsel_00.jpg)
- Open the keyless chuck.
- Check that the connection end of the accessory tool is clean and then insert it in the keyless chuck or, respectively, pull the accessory tool out of the keyless chuck.
- Retighten the keyless chuck.
Switching on
- Press the control switch.
Switching off
- Release the control switch.
Care and maintenance
- Keep the tool, especially its grip surfaces, clean and free from oil and grease.
- Do not use cleaning agents containing silicone.
- Never operate the power tool when the ventilation slots are blocked. Clean the air vents carefully using a dry brush. Do not permit foreign objects to enter the interior of the tool.
- Clean the outside of the tool at regular intervals with a slightly damp cloth. Do not use a spray, steam pressure cleaning equipment or running water for cleaning. This may negatively affect the electrical safety of the power tool.
Transport and storage
- Remove the battery before transporting or storing the drill.
- Observe the nationally and internationally applicable transport regulations when shipping batteries by road, rail, sea or air.
Troubleshooting
If the trouble you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, please contact Hilti Service.Trouble or fault |
Possible cause |
Action to be taken |
---|---|---|
The battery doesn’t engage with an audible double click. |
The retaining lugs on the battery are dirty. |
|
The control switch can’t be pressed, i.e. the switch is locked. |
The safety lock is engaged. |
|
The power tool doesn’t run. |
The battery is not fully inserted. |
|
The tool doesn’t work and one LED blinks. |
Low battery. |
|
The tool cuts out while operating, the 4 LEDs on the battery display blink. |
The overload cut-out has been activated. |
|
The overheating cut-out has been activated. |
|
|
The battery runs down more quickly than usual. |
Very low ambient temperature. |
|
The tool or battery gets very hot. |
The tool is overloaded (application limits exceeded). |
|
Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.